• Zarejestruj
  • Zaloguj

Aktualności

Print page

Nowości z Europy, Nowości z Japonii

Podaj oryginalne źródło

Aktualne publikacje

2018-05-17 – Effective control of water distribution networks and processing facilities

IFAT 2018, 14th –18th May 2018, Munich, Hall C1 / Stand 440 Since incomes for operating companies and government authorities in the water industry are either fixed or hard to change, reducing costs is a strong driving force behind any investment. At the IFAT exhibition 2018, Mitsubishi Electric is presenting its life-cycle management solutions that can support overall efficiency by reducing ...

Nowości z Europy, Nowości z Japonii

2018-05-16 – Optimised municipal water management by artificial intelligence

Process management, visualisation and control package Aquatoria® is delivering balanced water pressure across urban distribution networks, significantly improving water service levels, reducing leaks and lowering energy usage. The ideal situation for any water utility operator is to provide a service as close to perfect as possible.

2018-03-22 – Preview IFAT 2018 - Solutions for improving operations and reducing costs

As the water industry drives for increased efficiency in every area, completely integrated solutions that offer improvements to operational insight, energy usage, physical supply networks and process installations are of high importance. At the IFAT 2018 exhibition, Mitsubishi Electric will be presenting its approach to meeting these needs, which has been developed based on an understanding of ...

2018-02-27 – Faster time to market

Consistent data exchange between electrical wiring and control software through AutomationML Mitsubishi Electric has implemented the AutomationML interface within iQ Works, the integrated software suite for programming Mitsubishi Electric automation products. AutomationML represents an important step-change in the way complex equipment is designed ...

2017-11-30 – Full suite of special function CPUs for MELSEC iQ R PLC

Automation platform supports the digital transformation of manufacturing Mitsubishi Electric is highlighting the benefits of the PLC as a platform for automation, with a complete set of dedicated CPU modules for the MELSEC iQ R Series PLC. A CNC CPU module and a robot control CPU now complement the existing options for analogue and digital I/O, motion, positioning, process control, safety and ...

2017-11-29 – Quality management and digitalisation in manual assembly operations

At SPS IPC Drives 2017, Mitsubishi Electric’s Guided Operator Solutions for manual assembly applications will demonstrate how improvements in quality and productivity can be achieved. These solutions also enable the seamless transfer of production data from manual assembly operations to higher-level enterprise systems, supporting the digital transformation within manufacturing.

2017-11-29 – Mitsubishi Electric previews extension to its range with collaborative robot

Supporting humans with a full complement of robot features and equipment on board At SPS IPC Drives from 28 - 30 November 2017 in Nuremberg, Mitsubishi Electric is setting up a demonstration of production in an Industry 4.0 environment that will include a new collaborative robot, working together with an operator without safety barriers.

2017-11-28 – Be smart with digital transformation!

At this year’s event, Mitsubishi Electric is going to show visitors to the SPS IPC Drives show in Nuremberg how digitalisation can increase their production flexibility. In making use of integrated automation platforms new opportunities can be found for shop floor optimisation.

2017-11-28 – Flexible line integration delivered by modular Linear Transfer System and its Smart Carriages

Intelligent conveying system powered by on-board battery offers productivity advantages with unique safety concept.

2017-09-20 – Debut at EMO 2017 - New concept in robotics for predictive maintenance

EMO Hannover 2017, 18th – 23rd September 2017, Hannover, Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric is using EMO 2017 to demonstrate innovative predictive maintenance possibilities for robots that can reduce operational costs, increase asset productivity and improve process efficiency. The cloud-based solution is based on the AI platform within IBM Watson, which enables ...

2017-09-19 – Mitsubishi Electric next-generation CNC technology at EMO 2017

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric is addressing the need for fast, precise and affordable control of machine tools for complex machining applications with a new range of CNC systems. The M800 and M80 controllers offer superior functionality and intuitive usability...

2017-09-19 – Fraunhofer Institute and Mitsubishi Electric demonstrate human orientated machine operation at EMO 2017

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric is providing a glimpse of the future with human orientated monitoring and training for CNC-machines at EMO 2017, using smart devices offering direct integration with machine control systems. Developed as a pilot project with the Fraunhofer Institute for Production Technology IPT

2017-09-18 – Premiere at EMO - MV R Connect wire-cutting machines with new-generation control

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric announces the unveiling of two wire-cutting machines with a new control and simplified operation at EMO 2017.

2017-09-18 – Solutions for the digital transformation of production

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 In an increasingly competitive manufacturing environment, businesses need flexibility, improved productivity, and the capability to make gains in efficiency and reductions in downtime. Mitsubishi Electric is showing how these requirements can be met with a focus on connected production systems....

2017-08-21 – Mitsubishi Electric delivers solutions for digital transformation at EMO 2017

At the EMO exhibition in Hannover, visitors to Mitsubishi Electric’s stands can experience how to benefit from ongoing digitalisation at a manufacturing level. The theme “e F@ctory – pushing business further” covers a wide range of technologies aligned to current challenges in the machine building sector.

2017-08-08 – Smart Condition Monitoring aims to end downtime for the Food and Beverage Industry

Predictive maintenance is the best answer to minimising the risks of equipment failure, however, monitoring practices in the past have been expensive, problematic and at worst, unreliable. The solution is to switch to what Mitsubishi Electric offers to as ‘Smart Condition Monitoring’, a system which can connect to rotating equipment and provide plant-wide 24-7 monitoring.

2017-08-02 – Mitsubishi Electric Contributes e-F@ctory Demonstration Zone in Changshu Innovation Centre for Green & Intelligent Manufacturing

Supporting intelligent manufacturing in Chinese companies with e-F@ctory Mitsubishi Electric Corporation (TOKYO: 6503) has provided support and products for the recently completed e-F@ctory* demonstration zone within the Changshu Innovation Centre for Green & Intelligent Manufacturing, aimed at promoting intelligent manufacturing in China.

2017-07-25 – A Lion for three robots

Mitsubishi Electric’s interactive robotic installation known as “Threebots” has been awarded with the coveted Silver Lion in Cannes. “Threebots” has already received several awards since its installation at the German branch in Ratingen.

2017-06-20 – Mitsubishi Electric to Build Integrated Factory for VI/VCB Production

Mitsubishi Electric Corporation (TOKYO: 6503) announced in March that it would build an integrated factory for the production of vacuum interrupters (VI) and vacuum circuit breakers (VCB) at its Power Distribution Systems Center in Marugame, Japan. Operation is scheduled to start in July 2018.

2017-07-18 – The journey towards Industry 4.0

Hartmut Pütz, President Factory Automation EMEA at Mitsubishi Electric Europe, talks about the digital transformation of industry. He focuses on the effects on manufacturing businesses, especially at a production level, and how customers will benefit from innovative Mitsubishi Electric solutions.

2017-07-05 – Mitsubishi Electric Establishes FA Service Facilities in Querétaro and Monterrey, Mexico

Strengthening a nationwide network for servicing factory-automation products

2017-06-29 – Smart automation control platforms are essential for future power generation

Integration of new power generation sources as they develop over the next decade will require advanced automation to create intelligent systems and find increased efficiency on a macro and micro scale.

2017-06-28 – Power generation in the energy transition needs smart technology solutions

Some of the most important requirements for power generation in the energy transition period are increased flexibility and greater efficiency for staying competitive. These are being addressed by Mitsubishi Electric with a range of smart automation and electrical solutions.

2017-06-08 – Preview Power-Gen 2017: Smart solutions for power generation to support the energy transition

At POWER-GEN Europe 2017, Mitsubishi Electric will be presenting scalable automation and electrical solutions for the key issues faced by the power generation industry today. Requirements for increased flexibility and greater efficiency are both addressed, in addition to staying competitive during the energy transition process.

2017-05-10 – Industrial Sewing Machines Use the Industrial Internet of Things to Increase Quality and Boost Productivity

Texprocess 2017, Frankfurt am Main, 09th - 12th May 2017, Hall 5.1, Stand C46 The Automotive and Textile sectors are constantly facing more challenging customer requirements that are resulting in a new manufacturing approach. As for industrial sewing processes, Mitsubishi Electric’s sewing machines have recently been supplemented by automation technology offering increased intelligence...

2017-05-05 – Key technology supporting packaging applications on their journey to Industry 4.0

Mitsubishi Electric and APT Automation present latest developments in Linear Transfer Systems with Smart Carriage technology at interpack 2017.

2017-05-04 – Innovative solutions for Packaging machines support industry 4.0 drivers

Easier machine integration via PackML and programming using S/W function blocks are key themes. Today’s packaged goods manufacturers face challenges to reduce costs per package unit - using production lines that also need to be flexible and ready to accommodate new packaging machine solutions. At the same time, production lines...

2017-04-26 – Mitsubishi Electric highlights how digital transformation boosts productivity and improves OEE

On Booth D40 in Hall 17 at the Hannover Messe 2017, Mitsubishi Electric is showing automation solutions that address manufacturer requirements to boost productivity, increase flexibility and improve OEE. Demonstrations highlight how users can achieve this through plant-wide integration and transfer of data to the Cloud, with the importance of data defining the digital transformation of businesses.

2017-04-24 – SAP, Mitsubishi Electric Enable New IoT-Based Services for Manufacturing with SAP® Cloud Platform

SAP SE (NYSE: SAP) and Mitsubishi Electric Europe today announced SAP’s participation in Mitsubishi Electric e-F@ctory Alliance partner program. This partnership will enable Mitsubishi Electric’s automation solutions to operate fully with SAP® Cloud Platform...

2017-04-12 – Mitsubishi Electric launches the ‘Industrial Internet of Industrial Sewing Machines’

Visitors of the Texprocess can see how Industrial Internet of Things (IIoT) connectivity boosts productivity and increases quality for users of Mitsubishi Electric industrial sewing machines in the context of Industry 4.0.

2017-03-16 – Mitsubishi Electric at CeBIT 2017 - The Connected Car, Autonomous Driving and Internet of Things (IoT)

A system which creates precise 3D street maps for safe autonomous driving, a concept car which uses advanced driver assistance systems and an innovative communication application are some of the highlights at the Mitsubishi Electric stand A38/24 in Hall 4.

2017-01-03 – Mitsubishi Electric’s e-F@ctory Alliance is growing – APT Automation becomes the latest member

Mitsubishi Electric has recently welcomed APT Automation as member of the e-F@ctory Alliance. They are a key provider of automation and production technology solutions. The two businesses collaborate closely to address industry challenges such as improved productivity, increased overall equipment effectiveness and greater production line flexibility.

2016-12-13 – Mitsubishi Electric’s “Threebots” honoured with Red Dot Design Awards

In November, Mitsubishi Electric was presented with the “Best of the Best” and “Grand Prix 2016” awards at the prestigious Red Dot Gala. The prizes were awarded for the interactive “Threebots” robot application which can be found at the company’s German branch in Ratingen.

2016-12-08 – Mitsubishi Electric previews new Smart Carriage for linear transfer systems at SPS IPC Drives

Visitors to SPS IPC Drives 2016 had the first chance to see a brand new Smart Carriage technology from Mitsubishi Electric and APT Automation*. Developed to operate with a dedicated linear transfer system, the Smart Carriage delivers on-board intelligence plus integrated power for on-carriage equipment....

2016-12-07 – Industry 4.0 solutions centre stage for Mitsubishi Electric during SPS IPC Drives 2016

At the SPS IPC Drives Expo 2016, Mitsubishi Electric showcased a portfolio of integrated automation components and services developed to help customers realise their individual business objectives and make tomorrow’s business a success. Under the banner ‘e F@ctory, your journey to Industry 4.0’, Mitsubishi Electric gave visitors the opportunity to explore new application solutions that enable...

2016-11-03 – Guided Operator Solutions enhance quality control process for air conditioning manufacturer

The need to maximise quality, productivity and efficiency on production lines and in manual assembly cells is a challenge faced by much of manufacturing industry. It has been met at Mitsubishi Electric Air Conditioning Europe by employing Guided Operator Solutions from sister company Mitsubishi Electric, Factory Automation.

2016-10-31 – Solutions for Industry 4.0 presented by Mitsubishi Electric at SPS IPC Drives 2016

At the forthcoming SPS IPC Drives Expo Mitsubishi Electric is showcasing a portfolio of integrated automation components and services developed to help customers realise their individual business objectives. Visitors to this year’s booth can explore new application solutions that enable the automation and digitalization of industrial processes and also exchange ideas ...

2016-10-26 – Guided Operator Solutions improve quality and performance in assembly processes

Eliminating human mistakes is one of the main quality challenges facing manufacturing industry today. To overcome this challenge, Mitsubishi Electric has launched a set of Guided Operator Solutions dedicated to preventing mistakes in manual parts picking and assembly tasks. The system is field proven and is already enabling manufacturers from a variety of industries to actively improve...

2016-09-06 – Mitsubishi Electric’s ‘Threebots’ Interactive Robot Installation Receives Several Awards

Mitsubishi Electric’s interactive robotic installation known as ‘Threebots’ has received several coveted awards since its installation at the new German branch office in Ratingen. They include the ‘Cutting Edge Award’ presented by Adobe, and ‘FWA’ (thefwa.com) the latter of which was awarded by a jury of more than 200 experts in recognition of projects that use cutting-edge technology to ...

2016-08-25 – New Contact Image Sensor from Mitsubishi Electric is at VISION 2016 Expo

The new high-speed contact image sensor (CIS) offers a compact, distortion-free alternative to line scan cameras. It will be featured on the Stemmer Imaging GmbH exhibition stand E52 situated in Hall 1 at VISION 2016 in Stuttgart from 8-10 November and supported by Mitsubishi Electric representatives at the show.

2016-08-16 – New flush-mount HMI enables machine builders to promote their own brand identity

With the launch of the latest addition to the GOT2000 family of HMIs, Mitsubishi Electric has introduced a new style of operator interface. The open-frame, back mounting design enables machine builders to reinforce their own brand identity and provides a flush finish to the machine panel for a smarter, more stylish aesthetic.

2016-06-16 – Preview PowerGen - Building a predictable future for power generation

The power generation industry is facing up to increasingly demanding challenges, driven by requirements for increased flexibility, greater efficiency and improved predictability. At POWER-GEN Europe, Mitsubishi Electric will be showing visitors how its proven, safe and reliable solutions can address these key themes in the energy market.

2016-06-09 – Where Virtual meets Reality - creating and operating a Virtual Power Plant

The amount of electricity produced using renewable energy sources is subject to fluctuations, making the network unstable. Conventional power plants can be used to balance out the situation. However, the problem with these is their negative CO2 balance and lack of flexibility. Virtual power plants can ensure stability by automatically combining renewable energy sources based on availability.

2016-06-08 – The future of inverter drives in the water industry

The challenges facing the water industry include climate change, rising energy costs, tightening legislation, population growth and increasing usage per head. The use of automated systems in order to make pumps and processes work more efficiently is helping keep pace with these demands; however, what does the future hold for one ...

2016-06-07 – PMSX®pro Web Monitoring – Plant control at a glance

ME-Automation Projects GmbH, a sister company of Mitsubishi Electric, has introduced a new functionality called “PMSX®pro Web Monitoring” to expand the proven, future-oriented process control system PMSX®pro.

2016-06-01 – Preparing the water industry for the future: identifying and implementing trends

In order to remain fit for the future, water supply and distribution facilities need to set themselves special challenges and take future trends seriously. Topics such as system migration and modernisation, data capture and analysis or preventive maintenance are becoming increasingly important when it comes to ensuring a high level of plant availability and efficient operation.

2016-04-26 – Mitsubishi Electric Europe appoints new Directors for Process Automation and Energy Business

Mitsubishi Electric has invested to strengthen further the business for automation solutions in the process and power sectors with two new appointments. Morteza Seraj has become the new Director for Process Automation. He succeeds Louis Meyer in the position, while Meyer moves to head up a new business field within Mitsubishi Electric as Director, Energy Systems, EMEA, focusing on energy solutions

2016-04-21 – Preview IFAT - Making optimum use of sewage, waste and renewable resources

Mitsubishi Electric will be presenting its comprehensive engineering expertise as a provider of complete solutions for water, sewage, waste and raw materials management at IFAT 2016 (Hall A5.243). Numerous successfully implemented turnkey and customised EI&C projects, such as water/sewage systems as well as solutions for producing energy from waste, biomass or biogas will be demonstrated.

2016-04-28 – Mitsubishi Electric's iQ Platform and Standard PLC Open Function Blocks reduce time to market for packaging machines

Mitsubishi Electric will be using a tubular bag machine to demonstrate its packaging machine engineering expertise at Hanover Trade Fair. The trade fair application is based on Mitsubishi Electric's automation iQ Platform. The system uses predefined function blocks especially for packaging machines which can be used to set up control systems including HMIs quickly and easily. The program ...

2016-03-29 – Mitsubishi Electric to Strengthen Factory Automation presence in Southern Europe and Africa

Italy FA Centre and South Africa FA Centre Satellite to support manufacturers Mitsubishi Electric Europe B.V. has announced the opening of a new Factory Automation (FA) Centre in Italy and a Factory Automation (FA) Centre Satellite office in South Africa, intended to provide automation products services to Southern Europe and Africa. There are a large number of manufacturing companies in ...

2016-03-22 – Preparing pharmaceutical and medical technology for the future

Production environment requirements in the pharmaceutical and medical technology sectors are very high. Not least, the strict cleanroom criteria present a particular challenge. In order to survive in a highly competitive market, companies also need to make sure that they increase their production effectiveness and minimise costs. Current trends include process optimisation for the purpose of ...

2016-03-15 – Mitsubishi Electric integrates own Factory Automation products to optimise building management processes

The Factory Automation Division of Mitsubishi Electric Europe B.V. has installed an extensive range of building automation and security products in the newly built German Branch in Ratingen. The products and solutions can be used for a variety of applications, for example quantifying, measuring, displaying, recording and monitoring current and voltage flows around the building. All the data ...

2016-03-11 – Mitsubishi Electric officially opens new German Branch in Ratingen

Mitsubishi Electric has officially inaugurated its new German Branch in Ratingen with a ceremony that included many traditional Japanese elements. More than 16,000 m2 of office space will accommodate up to 750 employees.

2016-01-06 – Mitsubishi Electric Europe appoints Director for Food & Beverage and Consumer Packaged Goods sector

Malte Schlüter has been appointed as Director for Food & Beverage and Consumer Packaged Goods (CPG) of the Factory Automation - European Business Group at Mitsubishi Electric Europe. His role is to be multifaceted and includes taking care of global customers in this fast moving, highly competitive and demanding sector and supporting the regional sales team within their key account business.

2015-11-27 – New medium voltage inverter meets the challenges of today with the technology of tomorrow

Mitsubishi Electric are launching a range of innovative medium voltage inverter drives at SPS IPC Drives 2015 (Nuremberg 24-26 November 2015), which are designed for both the current and future energy needs of industry. The drives are compact and modular, allowing for flexible installation in confined areas and deliver industry-leading energy efficiency with advanced IGBTs ...

2015-11-27 – Safer and more productive interaction between humans and robots enabled by MELFA SafePlus and safety sensor technology

At SPS IPC Drives 2015, Mitsubishi Electric, together with its system partner MH Elektro-Steuerungstechnik, are presenting an industrial robot that enables humans and robots to work together more safely and effectively during large batch production within closely confined work cells. In order to do that, an industrial robot from the MELFA F series of Mitsubishi Electric has been equipped with...

2015-11-27 – SPS 2015 - Using global experience to make renewable and EFW power plants more efficient

Energy from Waste (EFW) plants around the world rely on automated systems from Mitsubishi Electric to optimise performance and ensure maximum levels of efficiency while also achieving rigorous environmental standards for emissions.

2015-11-27 – SPS IPC DRIVES 2015 - Mitsubishi Electric continues its record of innovation in automation technology

Mitsubishi Electric is presenting several innovations in key automation technologies at the SPS IPC Drives. These cutting edge technologies have been developed to enhance the productivity, efficiency and performance of production plants across all industrial sectors.

2015-10-23 – Mitsubishi Electric Europe B.V. further bolsters business in Norway

Mitsubishi Electric Europe B.V establishes Norwegian Branch by integrating its subsidiary MIBA AS Mitsubishi Electric Corporation(TOKYO: 6503) Mitsubishi Electric Corporation today announces that its European subsidiary, Mitsubishi Electric Europe B.V, has completed the integration of its former air conditioning distributor MIBA AS, acquired in July. In addition, from October 2015, the ...

2015-11-10 – Preview - The world of automation at SPS IPC Drives

Integrated solutions for manufacturing and production industries are increasingly becoming state-of-the-art. The demand for better quality products, almost immediate availability and more product variants is constantly growing: Traceability, OEE (Overall Equipment Effectiveness), and resource management for example are becoming increasingly important for innovative companies...

2015-10-27 – e-F@ctory Wins Technological Leadership Award for Implementing IIoT in Factory Automation

Mitsubishi Electric's e-F@ctory concept has just been honored by Frost & Sullivan as part of their annual Best Practice Awards. The award recognizes Mitsubishi Electric's e-F@ctory as providing enabling technology in the field of the “Industrial Internet of Things in Factory Automation”.

2015-10-15 – Italian EMO fair proves major success for Mitsubishi Electric

Visitor traffic on Mitsubishi Electric’s stand at the recent EMO exhibition was especially high this year as the company launched its new generation of computer numerical control (CNC), the M800/M80 Series. The novelty is working with an innovative operating concept based on a new, ultra high speed, CNC-specific central processor unit.

2015-11-03 – History and the future both influence the latest automated production innovations of today

Mitsubishi Electric will have many of its key technologies on show at the EMO Exhibition (Milan, Italy, 5-10 October 2015, Hall 3, Stand H18/L17), where experts will also be on hand for discussions and demonstrations.

2015-09-22 – Preview – EMO 2015, Milan, Italy 5.-10.10.2015 - Integrated automation solutions at EMO 2015

Manufacturing and production industries are set to see significant change as automation systems become more and more integrated. End users are increasingly demanding better quality products, almost immediate availability and more product variants. There is also a growing need for traceability, energy efficiency, resource management, and coordination across multiple production sites

2015-09-21 – Review – RWM Exhibition proves a hit for Mitsubishi Electric’s EFW plant control solutions

The RWM Exhibition is one of Europe’s leading events for the resource management industries including Energy from Waste (EFW). As an experienced supplier of turnkey Electrical, Instrumentation and Control (EI&C) projects to power generation plant operators around the world, Mitsubishi Electric attended the 2015 show to present its latest solutions and services for EFW plants and energy management.

2015-09-21 – Preview EMO - Mitsubishi Electric has it all under control at EMO 2015

Mitsubishi Electric will be demonstrating its integrated, multi-faceted approach to manufacturing and production automation at this year’s EMO Exhibition (Milan, Italy, 5-10 October, Hall 3, Stand H18/L17).

2015-09-17 – New control system for smaller plants is simple, robust and cost-effective

RWM exhibition, Birmingham, 15.-17.9.2015 The PMSX®micro is a control system designed specifically for use on smaller scale plants, such as renewable energy power plants. It runs on a single computer yet delivers proven control technology in an inexpensive and easily engineered package. It is being launched at the RWM Exhibition (Birmingham, 15-17 September 2015) by Mitsubishi Electric and ...

2015-09-17 – Full range of MV switchgear is proven for EFW and other generating plants

RWM exhibition, Birmingham, 15.-17.9.2015 Attention to every detail is vital in renewable energy and energy from waste (EFW) plants. They are major capital investments that must run reliably for decades, producing power (and heat in combined heat and power plants) on demand. The exemplary reliability of components from Mitsubishi Electric makes them an extremely good match for this type of ...

2015-09-17 – Controlling and protecting steam turbines

RWM exhibition, Birmingham, 15.-17.9.2015 Turbiset® Steam Turbine Control and Protection solution can be used with any manufacturer’s turbine, and is being demonstrated on Mitsubishi Electric’s exhibition stand (C50-D51 – in hall 4) at this year’s RWM exhibition.

2015-09-17 – Mapping the clearest route to project completion

RWM exhibition, Birmingham, 15.-17.9.2015 Whether it is for a small renewable energy plant or a full-scale power station, often the hardest part of a control engineering project is the start. A popular and market-proven tool from Mitsubishi Electric and its e-F@ctory partner Adroit Technologies not only makes the planning stage easier, but also helps reduce the time and cost to completion of...

2015-09-17 – New hybrid power source (HPS) energy management system can select best source while also reducing consumption by up to 30%

RWM exhibition, Birmingham, 15.-17.9.2015 Reducing energy consumption is just one part of an industrial company’s energy management strategy, it must also source or generate its energy competitively, while taking account of CSI and green initiatives which may affect the energy mix. This situation opens up the requirement for a solution that can make complex purchasing and management decisions..

2015-09-17 – Make renewable and EFW plants more efficient with the global experience of Mitsubishi Electric

RWM exhibition, Birmingham, 15.-17.9.2015 Energy from Waste (EFW) plants around the world rely on automated systems from Mitsubishi Electric to optimise performance and ensure the maximum levels of efficiency while also achieving rigorous environmental standards for emissions.

2015-07-22 – Mitsubishi Electric launches the new MELSEC iQ-F series compact PLC

Mitsubishi Electric has expanded its iQ range of PLCs with the compact MELSEC iQ-F series, building on the legacy of the market-leading FX platform and broadening the range of available applications with a comprehensive set of “built-in” functions that offer features only previously found as add-ons or which did not exist at all in this category of PLCs. Sharing many of its features and concepts..

2015-07-30 – Industry 4.0 in the Food and Beverage industry

The practical advantages that the new cyber-physical interface of Industry 4.0 brings are acknowledged by engineers across a range of industries. Jeremy Shinton, Product Manager UK – Business Solutions at Mitsubishi Electric Europe B.V., UK Branch, Automation Systems Division, explains how food and drink manufacturers in particular can benefit from the implementation of Industry 4.0:

2015-07-07 – New simple, robust and cost-effective distributed control system for smaller plants

Mitsubishi Electric and ME-Automation Projects, part of the Mitsubishi Electric Group, will launch a new distributed control system, the PMSX®micro, at the RWM exhibition this year. The new system is designed specifically for smaller scale applications. PMSX®micro runs on a single industrial computer and delivers proven control technology in an inexpensive and easily engineered package.

2015-06-30 – Mitsubishi Electric Europe shows how to get the most from waste to energy and renewable resources

Mitsubishi Electric has a proven track record of supplying turnkey Electrical, Instrumentation and Control (EI&C) projects for energy producers including full engineering and commissioning. This includes systems for Energy from Waste, Biomass and related industries, such as Biogas based generation for Waste Water clients – covering both electricity generation from steam turbines and district ...

2015-05-27 – Cyber-security: a journey, not a destination

Cyber-security has been a hot topic since the Stuxnet incident of a few years ago. Previously it was thought that securing the “top end” of an organisation was an adequate solution but this incident and others like it completely changed the security landscape and highlighted vulnerabilities in the de-facto automation architecture that previously had not been considered. Chris Evans ...

2015-05-19 – New office of Mitsubishi Electric Factory Automation in the Netherlands

Mitsubishi Electric’s successful global Factory Automation Group operates a network of sales offices and technology centres around the world - the latest of which, comprising a sales office and a dedicated training and technology facility in Mijdrecht near Amsterdam, will be officially opened on 28th May 2015.

2015-06-02 – Mitsubishi Electric Launches New Environmental Plan

Mitsubishi Electric Corporation announced 23rd of April that it has launched as of this month its eighth environmental plan, a three-year action plan aligned with a long-term environmental management vision pointing to 2021, Mitsubishi Electric’s centenary.

2015-05-28 – Mitsubishi Electric Europe B.V. Grows African business

Mitsubishi Electric Corporation announces the expansion of its business in Africa with the launch of a new Mitsubishi Electric Europe B.V. office in Johannesburg, South Africa.

2015-04-29 – Changes in the Top Management at Mitsubishi Electric

New President and CEO for Europe and new President of Mitsubishi Electric´s German Branch appointed Mitsubishi Electric announces the appointment of Yoji Saito to the role of President and CEO of the company’s European operations as of 1 April 2015. Based at Mitsubishi Electric’s European Corporate Office in Uxbridge, Mr. Saito’s new responsibilities include leading ...

2015-04-16 – Mitsubishi Electric and partners demonstrate hands-on handling solutions

At this year's Hannover Messe, Mitsubishi Electric and partners will be presenting hands-on handling and automation solutions. The focus will be on robotics including an integrated high-precision, flexible laser marking solution from Taufenbach GmbH, an automated screw application system from WSM-Automation GmbH, an application from Bilfinger HSG and Datalogic S.R.L. ...

2015-04-14 – Reduce your engineering costs by up to 50% with Mitsubishi Adroit Process Suite (MAPS) and Eplan Electric P8

At SPS IPC Drives 2014, Mitsubishi Electric demonstrated the integration of the Mitsubishi Adroit Process Suite (MAPS) with Eplan Electric P8 data for the first time, underlining the positioning of MAPS as an integrated automation lifecycle software solution. The integration enables Eplan Electric P8 users to generate a MAPS project directly from Eplan Electric P8 circuit diagrams.

2015-04-02 – Preview - Solutions for the water industry at the "PUMPENplatz"

Mitsubishi Electric will be presenting an innovative portfolio of solutions designed specially for the water industry at the "PUMPENplatz" at Hanover trade fair on Stand G43, Hall 15. Providing consumers with clean drinking water is a vital process but handling waste water correctly is also an extremely critical issue. Strict requirements such as the Urban Waste Water Treatment Directive provide..

2015-03-26 – Mitsubishi Electric Develops IoT Factory Controller for Future Factories

Collects factory data using IoT technology and collaborates with cloud Mitsubishi Electric Corporation (TOKYO: 6503) announces its Internet of Things (IoT) Factory Controller to connect e-F@ctory, the company’s factory automation (FA) solution, with the cloud for the emerging IoT ecosystem. IoT Factory Controller is now being verified in test operation, with commercialization targeted at ...

2015-03-02 – Preview Anuga - Complete solutions for the food and beverage industry from a single source

As a supplier of complete solutions, Mitsubishi Electric will be exhibiting its comprehensive range of products designed especially for the food and beverage industry at Anuga FoodTec in Hall 07.1, Stand A109. Visitors to the stand will also be able to witness the high-speed performance of the latest RH-F series overhead SCARA robot as it carries out a typical pick-and-place application....

2014-12-18 – New FA Product Showroom Established in Republic of Korea

Supporting Korean manufacturers by introducing new products to meet complex needs. Mitsubishi Electric Corporation has announced the establishment of a new showroom within the headquarters of Mitsubishi Electric Automation Korea Co., Ltd. (MEAK), a wholly owned Mitsubishi Electric Group subsidiary based in Seoul that handles sales and service of factory automation ...

2014-09-22 – Foundation stone laid at the site of Mitsubishi Electric’s new offices in Ratingen

Barely six months since the ground was broken for the new offices, a foundation stone has been laid at the site of the new German Branch of Mitsubishi Electric Europe in Balcke-Dürr-Allee, Ratingen. The ceremony, which was attended by the Mayor of Ratingen, Mr Klaus Pesch, followed tradition by sealing a time capsule into the foundations which contained amongst other things a German and Japanese..

2014-09-30 – Intel and Mitsubishi Electric collaborate to create next generation Factory Automation systems

Pilot program demonstrates the benefits of End-to-End Internet of Things (IoT) connectivity in industrial settings

2014-09-29 – Energy from Waste sector gets ready for expansion and development

Mitsubishi Electric’s first-time presence in the EfW (Energy from Waste) hall at the Resource Efficiency and Waste Management show (RWM) in Birmingham, UK, has been hailed as an immediate success.

2014-09-23 – Food & beverage production fit for the future: Productivity and efficiency achieved with innovative solutions from Mitsubishi Electric

The food and beverage industry faces major challenges. These include increasing product diversity, shorter product life cycles, fluctuating order quantities and stricter statutory regulations particularly with respect to hygiene directives, just to name a few. Continuous improvement of production processes and efficiency increases cost savings, optimises profit margins and ...

2014-09-11 – Mitsubishi Electric to Strengthen FA Product Services in Ahmedabad, India

Mitsubishi Electric Corporation announced on 2nd of September, that Mitsubishi Electric India Pvt. Ltd. has begun operating, effective immediately, a new centre to provide factory-automation (FA) services in Ahmedabad with the Indian state of Gujarat, where a large number of Japanese manufacturing companies in need of FA services are operating.

2014-08-13 – High-speed screw-fastening system from Engmatec on the Mitsubishi Electric stand

At this year’s Motek trade fair to be held from 6-9 October 2014 in Stuttgart, Mitsubishi Electric together with Engmatec GmbH will be presenting a high-speed screw-fastening station for inline operation as part of an assembly line (hall 7, stand 7210).

2014-08-05 – Mitsubishi Electric demonstrates world class capabilities in energy from waste

Mitsubishi Electric Europe will be exhibiting at RWM 2014 – the resource efficiency and waste management show, being held in the National Exhibition Centre, Birmingham UK, 16-18 September 2014. For more than 25 years Mitsubishi Electric has been one of the leading suppliers for the Energy from Waste (EfW) industry. It will be displaying its solutions on stand 4C44-D45 in hall 4 & 5 ...

2014-04-16 – Mitsubishi Electric Group to Acquire Setsuyo Astec Corporation

Mitsubishi Electric Corporation announced that the company and its group companies will acquire Setsuyo Astec Corporation, a factory automation (FA) equipment sales firm operating in 10 Asian countries and regions, to enhance Mitsubishi Electric’s presence in these markets. With Setsuyo Astec as a wholly owned subsidiary, Mitsubishi Electric expects to raise FA sales in Asia to 200 billion yen...

2014-05-15 – Making baked products manufacturing fit for the future: Productivity and efficiency through data transparency

Pressure on prices is rising in the bakery market. Of particular concern is the increasing pressure from the discounters who are competing with cheap products baked freshly in store. At the same time, productivity and profit margins are low in the food processing industry in comparison to other producing industries. Above all ...

2014-04-22 – Preview components 2014 - Mitsubishi Electric Europe and Robotronic exhibit world’s first syringe handling solution with a small footprint

At this year’s components show, which is being staged in parallel with interpack, Mitsubishi Electric Europe and Swiss robotics specialist Robotronic are jointly presenting a brand new handling solution for supplying pre-filled syringes to an end-of-line packing system. The unique concept takes up very little space, yet offers a high processing rate of up to 600 syringes per minute and ...

2014-04-04 – Mitsubishi Electric announces the opening of the MEU Branch in Dubai for the Automation Division

Mitsubishi Electric Europe, MEU, is expanding its business in the Middle East region announcing the opening of the new Branch for Automation Division in Dubai at Dubai Silicon Oasis.

2014-03-18 – Innovation in Packaging applications with Mitsubishi Electric’s Motion Control technology

Mitsubishi Electric is a world leader in the three principal application areas for servo drives in industrial automation: robotics, CNC and general motion control (GMC). Mitsubishi manufactures its own technologies in all of these fields, something which very few other manufacturers can match. Combining this capability with unmatched service results in control solutions enabling ...

2014-03-12 – IFAT preview - Mitsubishi Electric designs special water management solutions

At this year’s IFAT – the world’s leading trade fair for water, sewage, waste and raw materials management – Mitsubishi Electric, along with its subsidiary ME-Automation Projects GmbH (formerly KH-Automation Projects), will be presenting a range of innovative solutions designed for the water market. The two companies will be sharing Stand A5 425/524 in Hall 5.

2014-02-25 – Mitsubishi Electric Appoints New President & CEO, Chairman

Mitsubishi Electric Corporation appointed Masaki Sakuyama as the company’s new President & CEO, effective April 1, 2014. Masaki Sakuyama will replace Kenichiro Yamanishi, who will assume the position of Chairman.

2014-02-18 – Mitsubishi Electric goes live in EMEA with new Factory Automation global website concept

Mitsubishi Electric Europe offers its web visitors and customers an even better online experience, with the launch of its EMEA websites built upon Mitsubishi Electric’s Factory Automation Global Website Strategy. At the European portal eu3a.mitsubishielectric.com, as well as on 23 country websites, visitors will find a streamlined new website with a modern design ...

2014-01-28 – e-F@ctory Alliance welcome Eplan as new member

In parallel with Eplan joining the e-F@ctory Alliance, Mitsubishi Electric Europe have been welcomed into Eplan’s “Community of efficient engineering”. This was agreed between Maximilian Brandl, Chairman of Eplan’s board of Management, and Hartmut Pütz, President of Mitsubishi Electric’s European Factory Automation Business Group, during a meeting at the SPS IPC Drives fair 2013 in Nuremberg...

2013-11-26 – New FR-A770 690V frequency inverters: high performance in harsh environments

The new FR-A770 inverters – high-performance devices with an operating voltage of 690 volts – are Mitsubishi Electric’s latest additions to the tried and tested FR-A700 series. The FR-A770 inverters are based on the successful FR-A740-EC models and are ideally suited for use in harsh environments.

2013-11-26 – Mitsubishi Adroit Process Suite 3.0 perfects life cycle management

Mitsubishi Electric will be presenting the next generation, version 3.0, of MAPS (Mitsubishi Adroit Process Suite) at this year’s SPS IPC Drives (Hall 7, Stand 380). MAPS 3.0 is the optimised HMI/SCADA life cycle management software that offers virtually unlimited scalability for versatile use.

2013-12-12 – KH-Automation Projects GmbH becomes ME-Automation Projects GmbH

KH-Automation Projects GmbH, which has been part of Mitsubishi Electric Group since mid 2013, is changing its name on 1st January 2014 - subject to completion of the formalities for entry in the Trade Register - to ME-Automation Projects GmbH.

2013-12-12 – Mitsubishi provided a look at its future automation solutions at SPS IPC Drives 2013

At this year's SPS IPC Drives, Mitsubishi Electric provided visitors with a look into the future of its automation solutions. For the first time in Europe, the successors to the globally popular compact MELSEC FX PLC series and the latest generation modular MELSEC iQ Platform were on show, alongside the new GOT2000 series touch screen HMI and the new FR-A800 high-end frequency inverter range.

2013-11-26 – Mitsubishi Electric presents new modular control concept MELSEC iQ-R

Mitsubishi Electric will be presenting its new control concept, MELSEC iQ-R, for the first time in Europe at SPS IPC Drives 2013 in Nuremberg. Compared with its predecessor, the successful MELSEC System Q series, the new modular high-performance controller will significantly reduce development costs as well as maintenance and operating costs...

2013-11-26 – New MELSEC FX5 series from Mitsubishi Electric - the next generation of compact PLC

The new MELSEC FX5 series is the next generation of the successful compact PLC that Mitsubishi Electric will be launching on the market. The successor to the advanced and well-established MELSEC FX3 range will once more drastically increase plant productivity and reduce total operating costs as well as energy consumption...

2013-11-26 – New FR-A800 series of frequency inverters provides maximum drive performance for plant and machinery

One of the highlights on the Mitsubishi Electric stand at this year’s SPS IPC Drives will be the new-generation FR-A800 inverters. The ultramodern drive has been specially designed for use in classic plant and machinery and with its maximum output and performance, increased efficiency and productivity are guaranteed...

2013-11-26 – Guaranteed safety: New WS-V low-voltage circuit breakers in ASTA-certified switchgear cabinet system

The challenge for designers and installers of low-voltage switchgears and control units is how to meet the rigorous approval requirements for user protection and system safety under normal operating conditions, for example in the case of a short circuit or overvoltage, and also those for protection against misuse in general. The method for providing proof of this compliance based on type testing.

2013-11-22 – Company nxtControl - Distributed control specialist - strengthens

Mitsubishi Electric Europe’s network partnership of specialist automation companies has been expanded with the addition of nxtControl. They are market leading experts in hardware independent programming for distributed control systems.

2013-11-21 – AUVESY joins Mitsubishi Electric’s e-F@ctory Alliance

Company AUVESY GmbH & Co KG has joined the e-F@ctory Alliance, a partner initiative of Mitsubishi Electric Europe for offering market leading industrial automation solutions. The German company AUVESY, located in Landau, are experts in automated backup and version control of software used in manufacturing and production environments.

2013-11-11 – Next Generations – Experience the future live at SPS IPC Drives

At this year's SPS IPC Drives, Mitsubishi Electric will be giving visitors a closer look into the future of its automation solutions. For the first time in Europe, the successors to the compact MELSEC FX PLC series and the modular automation concept MELSEC iQ Platform, the brilliant HMI GOT2000 series and the FR-A800 high-end frequency inverter will be presented.

2013-11-07 – Mitsubishi Electric’s iQ Platform: full automation on one rack

Machine tool manufacturers have been successfully combining Mitsubishi Electric CNC and robot technology in their systems for years and consequently promoting unmanned production. The iQ Platform from Mitsubishi Electric permits not only the seamless combination of CNC and robot CPUs but also of PLC and Motion Control CPUs – an integrated solution that is unique throughout the industry...

2013-10-29 – Mega project uses Mitsubishi Electric controls to improve Sussex coast water quality

One of the most ambitious wastewater treatment projects in Europe, designed to process several towns’ wastewater and improve water quality along the Sussex coast, has been speeded along because of the ease of integration of Mitsubishi Electric control equipment.

2013-09-12 – Mitsubishi Electric launches new webstore for automation software

The new e-F@ctory Alliance software webstore is a first for the automation business and offers a huge range of incredibly useful ‘approved’ automation software and dedicated function blocks available for instant download. Programs on offer also include partner solutions that have been developed alongside Mitsubishi Electric to support users to find best practice solutions for their automation...

2013-06-10 – Serwonapędy MR-J4 Mitsubishi Electric produktem roku 2013 w kategorii „napędy i sterowanie ruchem”.

Najnowsza seria serwowzmacniaczy MR-J4 Mitsubishi Electric zdobyła prestiżową nagrodę „Produkt Roku” w kategorii napędy i sterowanie ruchem - w ramach dorocznego konkursu, organizowanego przez renomowany magazyn europejskiej branży przemysłowej, Control Engineering w Czechach.

2013-06-13 – Mitsubishi Electric sponsors WorldSkills Leipzig 2013

1000 trainees and skilled workers, 67 countries and regions, 46 official competitive disciplines, 200,000 visitors, 3000 specialists, 1000 journalists and 38 robots from Mitsubishi Electric – this is the vocational World Cup. From 2 to 7 July, the best skilled workers in the world will be competing at the WorldSkills Leipzig 2013 event by demonstrating their abilities in a wide variety of ...

2013-06-04 – e-F@ctory Alliance exhibition launches into the virtual world

The e-F@ctory Alliance* trade show is the first full exhibition to be staged using Mitsubishi Electric’s new virtual exhibition platform, and the first major virtual show to deliver a convincing and rewarding visitor experience.

2013-06-03 – Mitsubishi Electric finalizes strategic acquisition of KH-Automation Projects

Mitsubishi Electric Corporation (TOKYO: 6503) has finalized its acquisition of KH-Automation Projects GmbH, a subsidiary of Koop Holding Group. The parties completed the acquisition on 29th May 2013, with Mitsubishi Electric acquiring a 100% share of KH-Automation Projects GmbH, a long term strategic partner with over 50 years experience in industrial and process automation.

2013-04-18 – European marketing torch is handed over at Mitsubishi Electric Factory Automation

Mitsubishi Electric Factory Automation - European Business Group (FA-EBG) is pleased to announce that Klaus Petersen has been appointed as Director Marketing for the EMEA (Europe, Middle East, Africa) Region, succeeding Chris Hazlewood, who is moving on to Mitsubishi Electric Japan to pursue the next level of his career.

2013-04-26 – Mitsubishi Electric otworzyło w Polsce dywizję cięcia laserowego

Z dniem 1 stycznia 2013 roku firma Mitsubishi Electric Europe B.V. otworzyła nową dywizję wycinarek laserowych w regionie Europy Środkowo-Wschodniej. Dywizja LPM (ang. Laser Processing Machines) zlokalizowana jest w centrali Mitsubishi Electric w Balicach i odpowiada za współpracę z dystrybutorami, szkolenia techniczne i handlowe oraz zapewnienie pełnego serwisu wycinarek laserowych z poziomu...

2013-04-24 – Mitsubishi Electric and Raima create secure data handling process

Controlling and managing a complex system is difficult at any time. However, users in the process (ex. water, petro-chemical) and infrastructure industries such as surface rail, airports or underground metro systems have the added complexities of having to do the same over extreme distances with the possibility of 1000's of I/O points.

2013-04-17 – Mitsubishi Electric expands Factory Automation business in Scandinavia

Mitsubishi Electric Europe has announced that it will further strengthen and expand its Factory Automation (FA) business in Scandinavia and the Baltic States. In line with this strategy a new FA office has been established to extend local customer support for its Factory Automation business in this region. The new FA business unit is located in Lund, South of Sweden.

2013-04-15 – Energy Efficiency with Mitsubishi Electric and KH-Automation at WASSER BERLIN 2013

At the WASSER BERLIN INTERNATIONAL Show from 23 – 26 April 2013, Mitsubishi Electric and KH-Automation Projects will present automation solutions for the water sector. The two companies specialise in systems for the water, waste water and waste materials sectors. The focal points are energy efficiency, remote maintenance, preventative maintenance and condition monitoring.

2013-03-21 – Mitsubishi Electric takes second major step in Turkish automation market

Following the establishment of Mitsubishi Electric Turkey A.Ş. in January 2013 by Mitsubishi Electric Corporation, the Mitsubishi Electric Group has now acquired a 100% share-holding of its local Factory Automation distribution partner GENEL TEKNİK SİSTEMLER SANAYİ ve TİCARET ANONİM ŞİRKETİ (GTS). This important step in developing a firm commitment to the Turkish market follows a 21 year ....

2013-03-14 – Mitsubishi Electric Europe awards prizes to winners of ‘Best HMI Screen’ competition

Mitsubishi Electric Europe has announced the three winners of its “Best HMI screen competition” – two from Italy and one from the Czech Republic. The hugely popular and successful competition was held to find the most creative use of HMI screens in an application, with each winner receiving a Samsung tablet as a prize.

2013-03-05 – Mitsubishi Electric to Expand Factory Automation Business in India

Mitsubishi Electric Corporation (TOKYO: 6503) announced that its subsidiary Mitsubishi Electric India Pvt. Ltd. will host a new factory automation (FA) development center on its premises for business expansion in India. Launched on March 1, the Indian FA Development Center will strengthen R&D functions in the FA business to better meet needs in the growing Indian market and global market beyond.

2013-02-26 – Cyber safety – what happens next

The high profile incidents with the Stuxnet malware and vulnerable SCADA systems provided a timely reminder that we need to take effective measures to protect process control systems and infrastructure from attacks from cyberspace. Thomas Lantermann, Senior Business Development Manager at Mitsubishi Electric Europe, looks at where vulnerabilities lie and how the problem will be exacerbated...

2013-02-13 – Mitsubishi Electric optimises Irish waste water treatment and purification plants in record time

The aim of the operators of a waste water treatment plant and four associated purification plants in the East of Ireland was to reduce ongoing operating costs through modernisation. In order to do that, the plant was brought right up-to-date by installing Mitsubishi Electric automation components. This involved taking particularly diverse performance requirements into account as well as ...

2013-02-12 – The Production-integrated Enterprise in 2020

Globalisation, increasing customer sophistication and resource scarcity are all challenges facing the process industries, and by 2020 these will be even more acute. Meeting these challenges will depend on structures that will enable wholly automated planning, dynamic scheduling and fully optimised production processes to control unit production cost.

2013-01-24 – Water industry moves to less data, more information

Regulators are driving the water industry to adopt Whole Life Asset Management, as the best way to ensure overall efficiency, keep prices down and quality up. This has created a need, not for more data but for better information, so the recent ‘Driving Innovations in the Water Industry Conference’ hosted by Mitsubishi Electric Europe B.V.’s, UK Branch looked at how some companies...

2012-12-14 – Mitsubishi Electric Establishes Sales Company in Indonesia

Mitsubishi Electric Corporation (TOKYO: 6503) announced that it has established a sales company in Indonesia, named PT. Mitsubishi Electric Indonesia (Mitsubishi Electric Indonesia), to handle sales of air-conditioning systems, home appliances and factory automation (FA) beginning in March 2013.

2012-10-17 – ACCS - 20 lat z Mitsubishi Electric

AutoCont Control Systems, największy dystrybutor firmy Mitsubishi Electric na terenie Czech, świętuje dwudziestolecie współpracy, która pozwoliła zmodernizować i zautomatyzować produkcję w całym regionie.

2012-08-09 – Mitsubishi Electric otwiera nowy oddział automatyki przemysłowej i CNC w Brazylii

Tokio, 1 sierpnia 2012 – Mitsubishi Electric Corporation (TOKYO: 6503) poinformowało o utworzeniu nowego oddziału w São Paulo (Brazylia), w celu wzmocnienia sektora produktów CNC (computerized numerical controller) na rynku brazylijskim. Nowa spółka, MELCO CNC do Brasil Comércio e Serviços S.A., zamierza do marca 2016 roku osiągnąć roczną sprzedaż w wysokości 25 mln USD.

2012-05-27 – Zmiana w Zarządzie Mitsubishi Electric w regionie Europy Środkowo-Wschodniej

Mitsubishi Electric Factory Automation ma przyjemność poinformować, że stanowisko regionalnego Dyrektora Oddziału w Europie Środkowo- Wschodniej (region Central Eastern Europe) objął Hitoshi Namba.

2011-12-15 – NOWY SHOWROOM MITSUBISHI ELECTRIC

Mitsubishi Electric otworzyło zmodernizowane Centrum Automatyki Przemysłowej w siedzibie firmy w Balicach. Jest to pierwsze tak nowoczesne centrum wystawienniczo-edukacyjne w Polsce.

2011-09-03 – INEA RBT d.o.o. nowym partnerem strategicznym Mitsubishi Electric

W ramach kontynuacji dynamicznego rozwoju na rynku Europy Środkowo-Wschodniej, 19 września 2011 roku Mitsubishi Electric Factory Automation podpisało kolejną umowę dystrybutorską z nowo powstałą słoweńską spółką joint venture, INEA RBT d.o.o.

2011-08-02 – Mitsubishi Electric świętuje 30 lat sukcesów na rynku przetwornic częstotliwości

Mitsubishi Electric posiada ponad 30-letnie doświadczenie w dziedzinie rozwoju przetwornic częstotliwości i znajduje się w ścisłej czołówce firm, które potrafią najlepiej przekładać wymagania rynku na skuteczne rozwiązania oraz wytyczać trendy dla technologii napędów. Firma sprzedała już ponad 14 milionów przetwornic częstotliwości na całym świecie, co jest dowodem wysokiej jakości sprzętu

2011-03-16 – Mitsubishi Electric to Support Japan Earthquake Disaster Relief Effor

Tokyo, March 14, 2011 – Mitsubishi Electric Corporation announced today that Mitsubishi Electric Group companies will donate a total of 500 million yen to aid and support victims affected by the Tohoku Pacific Earthquake that struck on March 11, 2011.

2011-03-15 – Mitsubishi Electric Operations Affected by Tohoku Pacific Earthquake

Tokyo, March 15, 2011 – Mitsubishi Electric Corporation announced today that its two major business operations in the Tohoku region have sustained damage as a result of the Tohoku Pacific Earthquake, which struck on March 11, 2011. However, no significant injuries among employees have been reported.

2011-03-14 – Mitsubishi Electric to Support Japan Earthquake Disaster Relief Efforts

Mitsubishi Electric Corporation announced today that Mitsubishi Electric Group companies will donate a total of 500 million yen to aid and support victims affected by the Tohoku Pacific Earthquake that struck on March 11, 2011.

2011-02-01 – Dynamiczny rozwój Mitsubishi Electric na rynku Europy Środkowo-Wschodniej

W ramach kontynuacji dynamicznego rozwoju na rynku Europy Środkowo-Wschodniej, Mitsubishi Electric Europe B.V. rozpoczyna ścisłą współpracę z kolejnymi partnerami. Firmy SIMAP oraz Procont to kluczowi dystrybutorzy w dziedzinie automatyki przemysłowej na rynku słowackim.

Uwaga: wszystkie teksty oraz ilustracje są własnością Mitsubishi Electric i są chronione prawami autorskimi. Mogą one być dowolnie używane pod warunkiem, że są przeznaczone do sprawozdań i informacji na temat Mitsubishi Electric lub naszych produktów. Użycie tych tekstów i ilustracji do innych celów niż cele prasowe lub publikacje radiowe wymaga naszej wyraźnej zgody.

Zapytania
Kontakt
Baza Wiedzy
Pomoc

Automaticon 2018 to zaproszenie do wirtualnego świata
Więcej informacji