• Zarejestruj
  • Zaloguj

Aktualności

Print page

Sterowniki

Podaj oryginalne źródło

Aktualne publikacje

2017-11-30 – Full suite of special function CPUs for MELSEC iQ R PLC

Automation platform supports the digital transformation of manufacturing Mitsubishi Electric is highlighting the benefits of the PLC as a platform for automation, with a complete set of dedicated CPU modules for the MELSEC iQ R Series PLC. A CNC CPU module and a robot control CPU now complement the existing options for analogue and digital I/O, motion, positioning, process control, safety and ...

Sterowniki

2017-11-29 – Quality management and digitalisation in manual assembly operations

At SPS IPC Drives 2017, Mitsubishi Electric’s Guided Operator Solutions for manual assembly applications will demonstrate how improvements in quality and productivity can be achieved. These solutions also enable the seamless transfer of production data from manual assembly operations to higher-level enterprise systems, supporting the digital transformation within manufacturing.

2017-11-28 – Flexible line integration delivered by modular Linear Transfer System and its Smart Carriages

Intelligent conveying system powered by on-board battery offers productivity advantages with unique safety concept.

2017-09-20 – Debut at EMO 2017 - New concept in robotics for predictive maintenance

EMO Hannover 2017, 18th – 23rd September 2017, Hannover, Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric is using EMO 2017 to demonstrate innovative predictive maintenance possibilities for robots that can reduce operational costs, increase asset productivity and improve process efficiency. The cloud-based solution is based on the AI platform within IBM Watson, which enables ...

2017-09-19 – Mitsubishi Electric next-generation CNC technology at EMO 2017

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric is addressing the need for fast, precise and affordable control of machine tools for complex machining applications with a new range of CNC systems. The M800 and M80 controllers offer superior functionality and intuitive usability...

2017-09-18 – Premiere at EMO - MV R Connect wire-cutting machines with new-generation control

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric announces the unveiling of two wire-cutting machines with a new control and simplified operation at EMO 2017.

2017-09-18 – Solutions for the digital transformation of production

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 In an increasingly competitive manufacturing environment, businesses need flexibility, improved productivity, and the capability to make gains in efficiency and reductions in downtime. Mitsubishi Electric is showing how these requirements can be met with a focus on connected production systems....

2017-08-21 – Mitsubishi Electric delivers solutions for digital transformation at EMO 2017

At the EMO exhibition in Hannover, visitors to Mitsubishi Electric’s stands can experience how to benefit from ongoing digitalisation at a manufacturing level. The theme “e F@ctory – pushing business further” covers a wide range of technologies aligned to current challenges in the machine building sector.

2017-08-08 – Smart Condition Monitoring aims to end downtime for the Food and Beverage Industry

Predictive maintenance is the best answer to minimising the risks of equipment failure, however, monitoring practices in the past have been expensive, problematic and at worst, unreliable. The solution is to switch to what Mitsubishi Electric offers to as ‘Smart Condition Monitoring’, a system which can connect to rotating equipment and provide plant-wide 24-7 monitoring.

2017-06-29 – Smart automation control platforms are essential for future power generation

Integration of new power generation sources as they develop over the next decade will require advanced automation to create intelligent systems and find increased efficiency on a macro and micro scale.

2017-06-28 – Power generation in the energy transition needs smart technology solutions

Some of the most important requirements for power generation in the energy transition period are increased flexibility and greater efficiency for staying competitive. These are being addressed by Mitsubishi Electric with a range of smart automation and electrical solutions.

2017-06-08 – Preview Power-Gen 2017: Smart solutions for power generation to support the energy transition

At POWER-GEN Europe 2017, Mitsubishi Electric will be presenting scalable automation and electrical solutions for the key issues faced by the power generation industry today. Requirements for increased flexibility and greater efficiency are both addressed, in addition to staying competitive during the energy transition process.

2017-05-10 – Industrial Sewing Machines Use the Industrial Internet of Things to Increase Quality and Boost Productivity

Texprocess 2017, Frankfurt am Main, 09th - 12th May 2017, Hall 5.1, Stand C46 The Automotive and Textile sectors are constantly facing more challenging customer requirements that are resulting in a new manufacturing approach. As for industrial sewing processes, Mitsubishi Electric’s sewing machines have recently been supplemented by automation technology offering increased intelligence...

2017-04-24 – SAP, Mitsubishi Electric Enable New IoT-Based Services for Manufacturing with SAP® Cloud Platform

SAP SE (NYSE: SAP) and Mitsubishi Electric Europe today announced SAP’s participation in Mitsubishi Electric e-F@ctory Alliance partner program. This partnership will enable Mitsubishi Electric’s automation solutions to operate fully with SAP® Cloud Platform...

2017-01-12 – New C80 CPU unit enables full CNC production line integration

The new C80 CNC CPU unit mounts alongside an iQ-R Series PLC’s existing modules, allowing nanometre scale control over machine tool functions. When applied as part of an iQ-R Platform it contributes toward integrated control over an entire manufacturing production line. Not only does this improve overall performance, but due to ease of integration and a common programming environment -GX Works3...

2017-01-05 – Mitsubishi Electric enables a holistic approach to predictive maintenance

Mitsubishi Electric has further developed its condition monitoring technology for predictive maintenance. The solution builds on the capabilities of add-on smart sensors by integrating them with an intelligent sensor controller for a more holistic approach to condition monitoring.

2016-11-03 – Guided Operator Solutions enhance quality control process for air conditioning manufacturer

The need to maximise quality, productivity and efficiency on production lines and in manual assembly cells is a challenge faced by much of manufacturing industry. It has been met at Mitsubishi Electric Air Conditioning Europe by employing Guided Operator Solutions from sister company Mitsubishi Electric, Factory Automation.

2016-10-31 – Solutions for Industry 4.0 presented by Mitsubishi Electric at SPS IPC Drives 2016

At the forthcoming SPS IPC Drives Expo Mitsubishi Electric is showcasing a portfolio of integrated automation components and services developed to help customers realise their individual business objectives. Visitors to this year’s booth can explore new application solutions that enable the automation and digitalization of industrial processes and also exchange ideas ...

2016-10-26 – Guided Operator Solutions improve quality and performance in assembly processes

Eliminating human mistakes is one of the main quality challenges facing manufacturing industry today. To overcome this challenge, Mitsubishi Electric has launched a set of Guided Operator Solutions dedicated to preventing mistakes in manual parts picking and assembly tasks. The system is field proven and is already enabling manufacturers from a variety of industries to actively improve...

2016-06-16 – Preview PowerGen - Building a predictable future for power generation

The power generation industry is facing up to increasingly demanding challenges, driven by requirements for increased flexibility, greater efficiency and improved predictability. At POWER-GEN Europe, Mitsubishi Electric will be showing visitors how its proven, safe and reliable solutions can address these key themes in the energy market.

2016-06-07 – PMSX®pro Web Monitoring – Plant control at a glance

ME-Automation Projects GmbH, a sister company of Mitsubishi Electric, has introduced a new functionality called “PMSX®pro Web Monitoring” to expand the proven, future-oriented process control system PMSX®pro.

2016-06-01 – Preparing the water industry for the future: identifying and implementing trends

In order to remain fit for the future, water supply and distribution facilities need to set themselves special challenges and take future trends seriously. Topics such as system migration and modernisation, data capture and analysis or preventive maintenance are becoming increasingly important when it comes to ensuring a high level of plant availability and efficient operation.

2016-04-21 – Preview IFAT - Making optimum use of sewage, waste and renewable resources

Mitsubishi Electric will be presenting its comprehensive engineering expertise as a provider of complete solutions for water, sewage, waste and raw materials management at IFAT 2016 (Hall A5.243). Numerous successfully implemented turnkey and customised EI&C projects, such as water/sewage systems as well as solutions for producing energy from waste, biomass or biogas will be demonstrated.

2016-04-28 – Mitsubishi Electric's iQ Platform and Standard PLC Open Function Blocks reduce time to market for packaging machines

Mitsubishi Electric will be using a tubular bag machine to demonstrate its packaging machine engineering expertise at Hanover Trade Fair. The trade fair application is based on Mitsubishi Electric's automation iQ Platform. The system uses predefined function blocks especially for packaging machines which can be used to set up control systems including HMIs quickly and easily. The program ...

2016-03-22 – Preparing pharmaceutical and medical technology for the future

Production environment requirements in the pharmaceutical and medical technology sectors are very high. Not least, the strict cleanroom criteria present a particular challenge. In order to survive in a highly competitive market, companies also need to make sure that they increase their production effectiveness and minimise costs. Current trends include process optimisation for the purpose of ...

2016-03-15 – Mitsubishi Electric integrates own Factory Automation products to optimise building management processes

The Factory Automation Division of Mitsubishi Electric Europe B.V. has installed an extensive range of building automation and security products in the newly built German Branch in Ratingen. The products and solutions can be used for a variety of applications, for example quantifying, measuring, displaying, recording and monitoring current and voltage flows around the building. All the data ...

2015-11-27 – SPS 2015 - Using global experience to make renewable and EFW power plants more efficient

Energy from Waste (EFW) plants around the world rely on automated systems from Mitsubishi Electric to optimise performance and ensure maximum levels of efficiency while also achieving rigorous environmental standards for emissions.

2015-11-27 – SPS IPC DRIVES 2015 - Mitsubishi Electric continues its record of innovation in automation technology

Mitsubishi Electric is presenting several innovations in key automation technologies at the SPS IPC Drives. These cutting edge technologies have been developed to enhance the productivity, efficiency and performance of production plants across all industrial sectors.

2015-11-10 – Preview - The world of automation at SPS IPC Drives

Integrated solutions for manufacturing and production industries are increasingly becoming state-of-the-art. The demand for better quality products, almost immediate availability and more product variants is constantly growing: Traceability, OEE (Overall Equipment Effectiveness), and resource management for example are becoming increasingly important for innovative companies...

2015-11-03 – History and the future both influence the latest automated production innovations of today

Mitsubishi Electric will have many of its key technologies on show at the EMO Exhibition (Milan, Italy, 5-10 October 2015, Hall 3, Stand H18/L17), where experts will also be on hand for discussions and demonstrations.

2015-09-17 – New hybrid power source (HPS) energy management system can select best source while also reducing consumption by up to 30%

RWM exhibition, Birmingham, 15.-17.9.2015 Reducing energy consumption is just one part of an industrial company’s energy management strategy, it must also source or generate its energy competitively, while taking account of CSI and green initiatives which may affect the energy mix. This situation opens up the requirement for a solution that can make complex purchasing and management decisions..

2015-09-17 – Make renewable and EFW plants more efficient with the global experience of Mitsubishi Electric

RWM exhibition, Birmingham, 15.-17.9.2015 Energy from Waste (EFW) plants around the world rely on automated systems from Mitsubishi Electric to optimise performance and ensure the maximum levels of efficiency while also achieving rigorous environmental standards for emissions.

2015-07-22 – Mitsubishi Electric launches the new MELSEC iQ-F series compact PLC

Mitsubishi Electric has expanded its iQ range of PLCs with the compact MELSEC iQ-F series, building on the legacy of the market-leading FX platform and broadening the range of available applications with a comprehensive set of “built-in” functions that offer features only previously found as add-ons or which did not exist at all in this category of PLCs. Sharing many of its features and concepts..

2015-07-07 – New simple, robust and cost-effective distributed control system for smaller plants

Mitsubishi Electric and ME-Automation Projects, part of the Mitsubishi Electric Group, will launch a new distributed control system, the PMSX®micro, at the RWM exhibition this year. The new system is designed specifically for smaller scale applications. PMSX®micro runs on a single industrial computer and delivers proven control technology in an inexpensive and easily engineered package.

2015-06-30 – Mitsubishi Electric Europe shows how to get the most from waste to energy and renewable resources

Mitsubishi Electric has a proven track record of supplying turnkey Electrical, Instrumentation and Control (EI&C) projects for energy producers including full engineering and commissioning. This includes systems for Energy from Waste, Biomass and related industries, such as Biogas based generation for Waste Water clients – covering both electricity generation from steam turbines and district ...

2015-04-16 – Mitsubishi Electric and partners demonstrate hands-on handling solutions

At this year's Hannover Messe, Mitsubishi Electric and partners will be presenting hands-on handling and automation solutions. The focus will be on robotics including an integrated high-precision, flexible laser marking solution from Taufenbach GmbH, an automated screw application system from WSM-Automation GmbH, an application from Bilfinger HSG and Datalogic S.R.L. ...

2015-04-02 – Preview - Solutions for the water industry at the "PUMPENplatz"

Mitsubishi Electric will be presenting an innovative portfolio of solutions designed specially for the water industry at the "PUMPENplatz" at Hanover trade fair on Stand G43, Hall 15. Providing consumers with clean drinking water is a vital process but handling waste water correctly is also an extremely critical issue. Strict requirements such as the Urban Waste Water Treatment Directive provide..

2015-03-26 – Mitsubishi Electric Develops IoT Factory Controller for Future Factories

Collects factory data using IoT technology and collaborates with cloud Mitsubishi Electric Corporation (TOKYO: 6503) announces its Internet of Things (IoT) Factory Controller to connect e-F@ctory, the company’s factory automation (FA) solution, with the cloud for the emerging IoT ecosystem. IoT Factory Controller is now being verified in test operation, with commercialization targeted at ...

2015-02-24 – MELSEC iQ-R, enabling manufacturers to achieve a high speed, information driven, operation

Mitsubishi Electric is pleased to announce that its revolutionary next generation iQ Platform, the iQ-R Controller Series is now available. Today’s manufacturing environment is already complex and fraught with competitive challenges, but tomorrow, the year after and four years after that will be even more taxing, especially as manufacturers contemplate concepts such as Big Data and the IoT...

2015-02-12 – Standalone data logger provides simple monitoring of production quality, efficiency and throughput

Mitsubishi Electric has introduced a new standalone data logger, the NZ2DL, that combines extensive data logging capability with simple set up. Eliminating the need for a dedicated PC, the BOX Data Logger is easily installed in an existing system – even while equipment is running – and with a few simple settings begins logging of equipment to a CompactFlash (CF) card.

2015-02-05 – Coordinating virtual power plants intelligently

At this year's trade press days, Mitsubishi Electric focussed on renewable energies. In his expert presentation entitled "Virtual power plants–a reliable source of energy for the future", Dag Hoeft, Process Industry Technical Sales Consultant, Mitsubishi Electric Europe B.V., looks at backgrounds and trends in renewable energies, explains the significance of virtual power plants for the energy...

2014-05-15 – Making baked products manufacturing fit for the future: Productivity and efficiency through data transparency

Pressure on prices is rising in the bakery market. Of particular concern is the increasing pressure from the discounters who are competing with cheap products baked freshly in store. At the same time, productivity and profit margins are low in the food processing industry in comparison to other producing industries. Above all ...

2014-04-22 – Preview components 2014 - Mitsubishi Electric Europe and Robotronic exhibit world’s first syringe handling solution with a small footprint

At this year’s components show, which is being staged in parallel with interpack, Mitsubishi Electric Europe and Swiss robotics specialist Robotronic are jointly presenting a brand new handling solution for supplying pre-filled syringes to an end-of-line packing system. The unique concept takes up very little space, yet offers a high processing rate of up to 600 syringes per minute and ...

2014-03-18 – Innovation in Packaging applications with Mitsubishi Electric’s Motion Control technology

Mitsubishi Electric is a world leader in the three principal application areas for servo drives in industrial automation: robotics, CNC and general motion control (GMC). Mitsubishi manufactures its own technologies in all of these fields, something which very few other manufacturers can match. Combining this capability with unmatched service results in control solutions enabling ...

2014-03-12 – IFAT preview - Mitsubishi Electric designs special water management solutions

At this year’s IFAT – the world’s leading trade fair for water, sewage, waste and raw materials management – Mitsubishi Electric, along with its subsidiary ME-Automation Projects GmbH (formerly KH-Automation Projects), will be presenting a range of innovative solutions designed for the water market. The two companies will be sharing Stand A5 425/524 in Hall 5.

2013-12-12 – KH-Automation Projects GmbH becomes ME-Automation Projects GmbH

KH-Automation Projects GmbH, which has been part of Mitsubishi Electric Group since mid 2013, is changing its name on 1st January 2014 - subject to completion of the formalities for entry in the Trade Register - to ME-Automation Projects GmbH.

2013-12-12 – Mitsubishi provided a look at its future automation solutions at SPS IPC Drives 2013

At this year's SPS IPC Drives, Mitsubishi Electric provided visitors with a look into the future of its automation solutions. For the first time in Europe, the successors to the globally popular compact MELSEC FX PLC series and the latest generation modular MELSEC iQ Platform were on show, alongside the new GOT2000 series touch screen HMI and the new FR-A800 high-end frequency inverter range.

2013-11-26 – Mitsubishi Electric presents new modular control concept MELSEC iQ-R

Mitsubishi Electric will be presenting its new control concept, MELSEC iQ-R, for the first time in Europe at SPS IPC Drives 2013 in Nuremberg. Compared with its predecessor, the successful MELSEC System Q series, the new modular high-performance controller will significantly reduce development costs as well as maintenance and operating costs...

2013-11-26 – New MELSEC FX5 series from Mitsubishi Electric - the next generation of compact PLC

The new MELSEC FX5 series is the next generation of the successful compact PLC that Mitsubishi Electric will be launching on the market. The successor to the advanced and well-established MELSEC FX3 range will once more drastically increase plant productivity and reduce total operating costs as well as energy consumption...

2013-11-11 – Next Generations – Experience the future live at SPS IPC Drives

At this year's SPS IPC Drives, Mitsubishi Electric will be giving visitors a closer look into the future of its automation solutions. For the first time in Europe, the successors to the compact MELSEC FX PLC series and the modular automation concept MELSEC iQ Platform, the brilliant HMI GOT2000 series and the FR-A800 high-end frequency inverter will be presented.

2013-11-07 – Mitsubishi Electric’s iQ Platform: full automation on one rack

Machine tool manufacturers have been successfully combining Mitsubishi Electric CNC and robot technology in their systems for years and consequently promoting unmanned production. The iQ Platform from Mitsubishi Electric permits not only the seamless combination of CNC and robot CPUs but also of PLC and Motion Control CPUs – an integrated solution that is unique throughout the industry...

2013-10-29 – Mega project uses Mitsubishi Electric controls to improve Sussex coast water quality

One of the most ambitious wastewater treatment projects in Europe, designed to process several towns’ wastewater and improve water quality along the Sussex coast, has been speeded along because of the ease of integration of Mitsubishi Electric control equipment.

2013-07-18 – Mitsubishi Electric extends MELSEC FX3G Compact PLC with Ethernet Embedded CPU

Mitsubishi Electric has extended the capability of its MELSEC FX3G Compact PLC with the release of a new Ethernet embedded CPU – the FX3GE. Further, the new CPU also adds two analogue inputs and an analogue output. These new analogue and network features, combined with the power and expandability of the MELSEC FX3G mean the new Compact PLC can meet the needs of a wider range of applications.

2013-06-19 – Mitsubishi Electric PLCs provide control heart of AGVs at automotive engine block assembly plant

A leading automotive manufacturer is benefiting from increased production in its engine block assembly thanks to the use of automated guided vehicles (AGV) to transfer components to different stations within the assembly process. Key to the design operation of the AGVs are the modular MELSEC L series PLCs from Mitsubishi Electric.

2013-06-04 – e-F@ctory Alliance exhibition launches into the virtual world

The e-F@ctory Alliance* trade show is the first full exhibition to be staged using Mitsubishi Electric’s new virtual exhibition platform, and the first major virtual show to deliver a convincing and rewarding visitor experience.

2013-04-24 – Mitsubishi Electric and Raima create secure data handling process

Controlling and managing a complex system is difficult at any time. However, users in the process (ex. water, petro-chemical) and infrastructure industries such as surface rail, airports or underground metro systems have the added complexities of having to do the same over extreme distances with the possibility of 1000's of I/O points.

2013-04-15 – Energy Efficiency with Mitsubishi Electric and KH-Automation at WASSER BERLIN 2013

At the WASSER BERLIN INTERNATIONAL Show from 23 – 26 April 2013, Mitsubishi Electric and KH-Automation Projects will present automation solutions for the water sector. The two companies specialise in systems for the water, waste water and waste materials sectors. The focal points are energy efficiency, remote maintenance, preventative maintenance and condition monitoring.

2013-03-26 – Trends in control technology: is there a future for the PLC?

Change defines the world. The current challenges faced by society range from the demographic shift to a growing scarcity of natural resources. Automation, too, is changing: future trends in control technology suggest that the role of that control technology will change...The experts at Mitsubishi Electric believe in the coexistence of both systems and already offer flexible, future-ready solution.

2013-03-05 – Smart conveyor lines up quiches for precision baking

In the drive to reduce packaging and its resultant waste, a specialist machinery builder has developed a pressureless queuing conveyor for collating quiches prior to baking.

2013-02-26 – Cyber safety – what happens next

The high profile incidents with the Stuxnet malware and vulnerable SCADA systems provided a timely reminder that we need to take effective measures to protect process control systems and infrastructure from attacks from cyberspace. Thomas Lantermann, Senior Business Development Manager at Mitsubishi Electric Europe, looks at where vulnerabilities lie and how the problem will be exacerbated...

2013-02-13 – Mitsubishi Electric optimises Irish waste water treatment and purification plants in record time

The aim of the operators of a waste water treatment plant and four associated purification plants in the East of Ireland was to reduce ongoing operating costs through modernisation. In order to do that, the plant was brought right up-to-date by installing Mitsubishi Electric automation components. This involved taking particularly diverse performance requirements into account as well as ...

2013-02-12 – The Production-integrated Enterprise in 2020

Globalisation, increasing customer sophistication and resource scarcity are all challenges facing the process industries, and by 2020 these will be even more acute. Meeting these challenges will depend on structures that will enable wholly automated planning, dynamic scheduling and fully optimised production processes to control unit production cost.

2013-01-24 – Water industry moves to less data, more information

Regulators are driving the water industry to adopt Whole Life Asset Management, as the best way to ensure overall efficiency, keep prices down and quality up. This has created a need, not for more data but for better information, so the recent ‘Driving Innovations in the Water Industry Conference’ hosted by Mitsubishi Electric Europe B.V.’s, UK Branch looked at how some companies...

2012-12-13 – Mitsubishi Electric Europe improves PLC-based data logging

In the push for increased overall equipment effectiveness (OEE), reduced energy usage, improved traceability, analysis of key performance indicators and more, the vital ingredient is data. Barry Weller, Product Manager-iQ Platform, Automation Systems Division of Mitsubishi Electric Europe’s UK Branch discusses why data logging has become an essential feature of modern production line and why...

2011-08-02 – Mitsubishi Electric świętuje 30 lat sukcesów na rynku przetwornic częstotliwości

Mitsubishi Electric posiada ponad 30-letnie doświadczenie w dziedzinie rozwoju przetwornic częstotliwości i znajduje się w ścisłej czołówce firm, które potrafią najlepiej przekładać wymagania rynku na skuteczne rozwiązania oraz wytyczać trendy dla technologii napędów. Firma sprzedała już ponad 14 milionów przetwornic częstotliwości na całym świecie, co jest dowodem wysokiej jakości sprzętu

2011-05-31 – Redukcja kosztów i zwiększenie jakości produkcji dzięki inżynierskiemu narzędziu firmy Mitsubishi Electric - MAPS

Partner firmy Mitsubishi Electric i e‑F@ctory, Adroit Technologies rozwiązał problem tradycyjnych narzędzi integracyjnych PLC-SCADA, stosując pakiet MAPS - Mitsubishi Adroit Process Suite. To kompletne narzędzie do automatyzacji całego cyklu życia produktu jest niezwykle przydatne w fazie projektowania i integracji projektu.

2011-02-01 – Dynamiczny rozwój Mitsubishi Electric na rynku Europy Środkowo-Wschodniej

W ramach kontynuacji dynamicznego rozwoju na rynku Europy Środkowo-Wschodniej, Mitsubishi Electric Europe B.V. rozpoczyna ścisłą współpracę z kolejnymi partnerami. Firmy SIMAP oraz Procont to kluczowi dystrybutorzy w dziedzinie automatyki przemysłowej na rynku słowackim.

Uwaga: wszystkie teksty oraz ilustracje są własnością Mitsubishi Electric i są chronione prawami autorskimi. Mogą one być dowolnie używane pod warunkiem, że są przeznaczone do sprawozdań i informacji na temat Mitsubishi Electric lub naszych produktów. Użycie tych tekstów i ilustracji do innych celów niż cele prasowe lub publikacje radiowe wymaga naszej wyraźnej zgody.

Zapytania
Kontakt
Baza Wiedzy
Pomoc

Automaticon 2018 to zaproszenie do wirtualnego świata
Więcej informacji