• Zarejestruj
  • Zaloguj

Aktualności

Print page

Inne produkty

Podaj oryginalne źródło

Aktualne publikacje

2017-11-29 – Quality management and digitalisation in manual assembly operations

At SPS IPC Drives 2017, Mitsubishi Electric’s Guided Operator Solutions for manual assembly applications will demonstrate how improvements in quality and productivity can be achieved. These solutions also enable the seamless transfer of production data from manual assembly operations to higher-level enterprise systems, supporting the digital transformation within manufacturing.

Inne produkty

2017-11-28 – Flexible line integration delivered by modular Linear Transfer System and its Smart Carriages

Intelligent conveying system powered by on-board battery offers productivity advantages with unique safety concept.

2017-09-19 – Mitsubishi Electric next-generation CNC technology at EMO 2017

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric is addressing the need for fast, precise and affordable control of machine tools for complex machining applications with a new range of CNC systems. The M800 and M80 controllers offer superior functionality and intuitive usability...

2017-09-19 – Fraunhofer Institute and Mitsubishi Electric demonstrate human orientated machine operation at EMO 2017

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric is providing a glimpse of the future with human orientated monitoring and training for CNC-machines at EMO 2017, using smart devices offering direct integration with machine control systems. Developed as a pilot project with the Fraunhofer Institute for Production Technology IPT

2017-09-18 – Premiere at EMO - MV R Connect wire-cutting machines with new-generation control

EMO Hannover 2017, 18th – 23rd September 2017, Hannover Hall 13 / Stand C85 and Hall 25 / Stand B94 Mitsubishi Electric announces the unveiling of two wire-cutting machines with a new control and simplified operation at EMO 2017.

2017-08-21 – Mitsubishi Electric delivers solutions for digital transformation at EMO 2017

At the EMO exhibition in Hannover, visitors to Mitsubishi Electric’s stands can experience how to benefit from ongoing digitalisation at a manufacturing level. The theme “e F@ctory – pushing business further” covers a wide range of technologies aligned to current challenges in the machine building sector.

2017-06-29 – Smart automation control platforms are essential for future power generation

Integration of new power generation sources as they develop over the next decade will require advanced automation to create intelligent systems and find increased efficiency on a macro and micro scale.

2017-06-28 – Power generation in the energy transition needs smart technology solutions

Some of the most important requirements for power generation in the energy transition period are increased flexibility and greater efficiency for staying competitive. These are being addressed by Mitsubishi Electric with a range of smart automation and electrical solutions.

2017-06-08 – Preview Power-Gen 2017: Smart solutions for power generation to support the energy transition

At POWER-GEN Europe 2017, Mitsubishi Electric will be presenting scalable automation and electrical solutions for the key issues faced by the power generation industry today. Requirements for increased flexibility and greater efficiency are both addressed, in addition to staying competitive during the energy transition process.

2017-05-05 – Key technology supporting packaging applications on their journey to Industry 4.0

Mitsubishi Electric and APT Automation present latest developments in Linear Transfer Systems with Smart Carriage technology at interpack 2017.

2017-05-04 – Innovative solutions for Packaging machines support industry 4.0 drivers

Easier machine integration via PackML and programming using S/W function blocks are key themes. Today’s packaged goods manufacturers face challenges to reduce costs per package unit - using production lines that also need to be flexible and ready to accommodate new packaging machine solutions. At the same time, production lines...

2017-04-12 – Mitsubishi Electric launches the ‘Industrial Internet of Industrial Sewing Machines’

Visitors of the Texprocess can see how Industrial Internet of Things (IIoT) connectivity boosts productivity and increases quality for users of Mitsubishi Electric industrial sewing machines in the context of Industry 4.0.

2016-12-08 – Mitsubishi Electric previews new Smart Carriage for linear transfer systems at SPS IPC Drives

Visitors to SPS IPC Drives 2016 had the first chance to see a brand new Smart Carriage technology from Mitsubishi Electric and APT Automation*. Developed to operate with a dedicated linear transfer system, the Smart Carriage delivers on-board intelligence plus integrated power for on-carriage equipment....

2016-08-25 – New Contact Image Sensor from Mitsubishi Electric is at VISION 2016 Expo

The new high-speed contact image sensor (CIS) offers a compact, distortion-free alternative to line scan cameras. It will be featured on the Stemmer Imaging GmbH exhibition stand E52 situated in Hall 1 at VISION 2016 in Stuttgart from 8-10 November and supported by Mitsubishi Electric representatives at the show.

2016-06-16 – Preview PowerGen - Building a predictable future for power generation

The power generation industry is facing up to increasingly demanding challenges, driven by requirements for increased flexibility, greater efficiency and improved predictability. At POWER-GEN Europe, Mitsubishi Electric will be showing visitors how its proven, safe and reliable solutions can address these key themes in the energy market.

2016-06-07 – PMSX®pro Web Monitoring – Plant control at a glance

ME-Automation Projects GmbH, a sister company of Mitsubishi Electric, has introduced a new functionality called “PMSX®pro Web Monitoring” to expand the proven, future-oriented process control system PMSX®pro.

2016-05-31 – New solution from Mitsubishi Electric

High-speed contact image sensor offers compact, distortion-free alternative to line scan cameras. Mitsubishi Electric has responded to the needs of the surface inspection market, in particular within the print industry, with the launch of a high-speed version of its contact image sensor (CIS), distributed under the name Mitsubishi Electric Line Scan Bar...

2015-11-03 – History and the future both influence the latest automated production innovations of today

Mitsubishi Electric will have many of its key technologies on show at the EMO Exhibition (Milan, Italy, 5-10 October 2015, Hall 3, Stand H18/L17), where experts will also be on hand for discussions and demonstrations.

2015-09-17 – New control system for smaller plants is simple, robust and cost-effective

RWM exhibition, Birmingham, 15.-17.9.2015 The PMSX®micro is a control system designed specifically for use on smaller scale plants, such as renewable energy power plants. It runs on a single computer yet delivers proven control technology in an inexpensive and easily engineered package. It is being launched at the RWM Exhibition (Birmingham, 15-17 September 2015) by Mitsubishi Electric and ...

2015-09-17 – Full range of MV switchgear is proven for EFW and other generating plants

RWM exhibition, Birmingham, 15.-17.9.2015 Attention to every detail is vital in renewable energy and energy from waste (EFW) plants. They are major capital investments that must run reliably for decades, producing power (and heat in combined heat and power plants) on demand. The exemplary reliability of components from Mitsubishi Electric makes them an extremely good match for this type of ...

2015-09-17 – Controlling and protecting steam turbines

RWM exhibition, Birmingham, 15.-17.9.2015 Turbiset® Steam Turbine Control and Protection solution can be used with any manufacturer’s turbine, and is being demonstrated on Mitsubishi Electric’s exhibition stand (C50-D51 – in hall 4) at this year’s RWM exhibition.

2015-09-17 – New hybrid power source (HPS) energy management system can select best source while also reducing consumption by up to 30%

RWM exhibition, Birmingham, 15.-17.9.2015 Reducing energy consumption is just one part of an industrial company’s energy management strategy, it must also source or generate its energy competitively, while taking account of CSI and green initiatives which may affect the energy mix. This situation opens up the requirement for a solution that can make complex purchasing and management decisions..

2015-09-17 – Make renewable and EFW plants more efficient with the global experience of Mitsubishi Electric

RWM exhibition, Birmingham, 15.-17.9.2015 Energy from Waste (EFW) plants around the world rely on automated systems from Mitsubishi Electric to optimise performance and ensure the maximum levels of efficiency while also achieving rigorous environmental standards for emissions.

2014-09-29 – Energy from Waste sector gets ready for expansion and development

Mitsubishi Electric’s first-time presence in the EfW (Energy from Waste) hall at the Resource Efficiency and Waste Management show (RWM) in Birmingham, UK, has been hailed as an immediate success.

2013-06-04 – e-F@ctory Alliance exhibition launches into the virtual world

The e-F@ctory Alliance* trade show is the first full exhibition to be staged using Mitsubishi Electric’s new virtual exhibition platform, and the first major virtual show to deliver a convincing and rewarding visitor experience.

2013-04-26 – Mitsubishi Electric otworzyło w Polsce dywizję cięcia laserowego

Z dniem 1 stycznia 2013 roku firma Mitsubishi Electric Europe B.V. otworzyła nową dywizję wycinarek laserowych w regionie Europy Środkowo-Wschodniej. Dywizja LPM (ang. Laser Processing Machines) zlokalizowana jest w centrali Mitsubishi Electric w Balicach i odpowiada za współpracę z dystrybutorami, szkolenia techniczne i handlowe oraz zapewnienie pełnego serwisu wycinarek laserowych z poziomu...

2011-02-01 – Dynamiczny rozwój Mitsubishi Electric na rynku Europy Środkowo-Wschodniej

W ramach kontynuacji dynamicznego rozwoju na rynku Europy Środkowo-Wschodniej, Mitsubishi Electric Europe B.V. rozpoczyna ścisłą współpracę z kolejnymi partnerami. Firmy SIMAP oraz Procont to kluczowi dystrybutorzy w dziedzinie automatyki przemysłowej na rynku słowackim.

Uwaga: wszystkie teksty oraz ilustracje są własnością Mitsubishi Electric i są chronione prawami autorskimi. Mogą one być dowolnie używane pod warunkiem, że są przeznaczone do sprawozdań i informacji na temat Mitsubishi Electric lub naszych produktów. Użycie tych tekstów i ilustracji do innych celów niż cele prasowe lub publikacje radiowe wymaga naszej wyraźnej zgody.

Zapytania
Kontakt
Baza Wiedzy
Pomoc