Główna treść

  • Zarejestruj
  • Zaloguj

Factory Automation

Print page

Factory Automation

Produkty & Rozwiązania

Rozwiązania

Pokaż wszystko

Produkty

2019-06-14
Six times more thermo-packaging machines can fit into the same space - The new Shawpak thermo-packaging machine developed by Riverside Medical Packaging allows manufacturers to replace a 20m long packing line with a single unit under 2m in length. A compact integrated control system developed by Mitsubishi Electric is key to optimising the machine’s performance while keeping within a small target size envelope.
2019-05-21
Integrating renewable sources into a reliable power ecosystem - Balancing different sources of power, including renewables represents the most efficient and sustainable approach to meeting the energy needs we have now, and those of the next generation. Efficient control hardware combined with the management and optimization offered by virtual power plants provides an opportunity to meet that challenge today.
2019-05-16
Muntons - Barley malt producer increases productivity with smart condition monitoring - Muntons, one of the UK’s largest producers of malted barley protect vital parts of their production process against unscheduled downtime by using the Smart Condition Monitoring (SCM) system from Mitsubishi Electric.
2019-04-10
Mitsubishi Electric launches HMI for extreme environments - With an extended operating temperature range of -20°C to +65°C, and protection ratings to IP67F/IP66F, the GOT2507T-WTSD 7” operator terminal meets the needs of harsh and demanding applications. No additional protective measures are required for washdown with high pressure water or use in power equipment that is typically located outdoors. As a result, it is a perfect fit...
2019-04-01
New performance inverters for applications with high power requirements - Mitsubishi Electric has extended its inverter portfolio with a 690V version of its FR-A800 series inverters. The new models of the FR-A870 690V line cover power outputs up to 1.5 MW. Yet this increased power is delivered in a slim package that starts at just 380mm wide, offering significant space saving potential. Furthermore, the FR-A870 line combines this high-power performance with features ...

Pokaż wszystko


Pierwsze kroki z CNC - szkolenie podczas ITM 2019 – Zapraszamy do zapisania się na darmowe warsztaty "Twoje pierwsze kroki z CNC", które odbywać się będą podczas targów ITM w Poznaniu.
Zapisz się na warsztaty

Mitsubishi Electric News – Odwiedź naszego bloga! - Kursy - Kalendarz seminariów - Referencje
Wejdź na bloga

Contact Image Sensors – Optymalny zapis obrazu dzięki zaawansowanej technologii CIS
CIS
Do góry